- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I'm working on a project where I need to set the CAN_ID of a FULL CAN mailbox at runtime (because the ID is coming from an EEPROM). Using the following topic (http://www.cypress.com/forum/psoc-3-architecture/modifying-full-can-mailbox-s-identifier-program) I was able to set my Tx FULL mailboxes appropriately to transmit with the appropriate ID.
However when I try the same pattern for CAN full Rx mailboxes it doesn't work:
The Tx Address updates properly, but the interrupt associated with that mailbox (mailbox 2) still triggers on the default ID the CAN component was compiled with (in this case 0x601) and not the 0x6BE I set the register to. This leads me to think that the ID of an full Rx mailbox isn't used as a mask, or if it is, it's configured at compile or initialization time and not updated later.
Does anyone know how I can do this? Should I be setting the mask register somehow? Setting that register before I initalize the CAN componenet?
- Labels:
-
PSoC 5LP
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Can you please share your project so that I check the CAN settings?