cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

GPIOs can provide only 4mA of current and sink 8mA. Can I connect multiple pins to generate a current of more than 4mA.

   

So, if i want a current of 20mA can I connect 5 pins together to provide this current???

   

And also when I require 20mA to be sinked can I connect 3 pins together to sink in the current??

0 Likes
7 Replies