cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 5, 3 & 1

Anonymous
Not applicable

GPIOs can provide only 4mA of current and sink 8mA. Can I connect multiple pins to generate a current of more than 4mA.

   

So, if i want a current of 20mA can I connect 5 pins together to provide this current???

   

And also when I require 20mA to be sinked can I connect 3 pins together to sink in the current??

0 Likes
7 Replies
Bob_Marlowe
Expert II

I have seen designs that use connected IO-pins to increase current with PSoC1 to 5. Take care, not to exceed the max. power dissipation for a port or a quadrant. Have a look into the datasheet.

   

 

   

Bob

0 Likes
ETRO_SSN583
Esteemed Contributor

Per CY8C55 datasheet you are limited to 20 mA source, 100 mA sink,

   

per Vddio supply pin, eg. respective GPIO port.

   

 

   

Regards, Dana.

0 Likes
Anonymous
Not applicable

Gpio pins provide very less amount of current

   

use GPIO pins in sinking mode with Vcc

0 Likes
ETRO_SSN583
Esteemed Contributor

So there is no confusion, when I posted

   

 

   

"Per CY8C55 datasheet you are limited to 20 mA source, 100 mA sink,

   

per Vddio supply pin, eg. respective GPIO port."

   

 

   

Thats for all pins in that port. So you can parallel to get to that limit, but do not

   

exceed the port limits (sum of all pin currents, Iol or Ioh).

   

 

   

Regards, Dana."

0 Likes
Anonymous
Not applicable
microHari 
   

 

   

Yes you can do it. You can try to use the pins of different quadrants so that you will not reach the maximum limit of quadrant's sourcing & sinking capability.

   

 

   

What exactly are you trying to do for 20mA sinking/sourcing?

0 Likes
ETRO_SSN583
Esteemed Contributor

One other approach is to recognize the min max specs are at a specific

   

Vol, Voh. Attached typical graphs show you can get 20 mA out of a pin at

   

other than worst case logic level voltages. Because the graphs are typicals,

   

use a worst case fudge factor of 50 100% on V. The implication is that

   

would cover all process and temp variations.

   

 

   

So for 20 mA sink, the typ output V is .3V, so double that for design purposes at

   

20mA. So can your circuit tolerate a Voh 0f .6V ?

   

 

   

Regards, Dana.

0 Likes
ETRO_SSN583
Esteemed Contributor

Actually a safer approach, the Vol spec is 8 mA at .6 Vol. From the graph at 8 mA

   

the typ curve reads ~ .2V (5V Vdd). So the multiplying factor woud be 3. So at

   

20 mA typ is ~ .4, so use 1.2 V as a worst case Vol at 20 mA.

   

 

   

This approach is better because graphs represent overall device behaviour. Note

   

the graphs are at 25 degrees C, so a better plan is still plan on paralleling, to cover

   

margin on temp effects, but you should be able to parallel less pins.

   

 

   

The Voh case a little tougher because the drive has source bulk effect added to its

   

drive problem, eg. more variation, lower Voh worst case

   

 

   

So in short, parallel pins as best worst case approach, if running out of pins consider

   

the above.

   

 

   

Regards, Dana.

0 Likes