cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

Dear Friends

   

I met an issue when supporting a customer.That is:
In the customer's hardware system now,the power supply and ground of the analog chips and microcontroller are separate.Except that the digital interface between evevry analog chip(like ADC) and MCU are isolated by
Photo-Coupler.These are just like picture attached.
But if we embed our PSOC5 in the circuit and replace the present analog chips and MCU,the main worry of customer is that how can the analog and digital be entirely separated.
I know that the power supply and ground of the analog block and digital block are separated. But I don't know how do the analog block and digital BUS ,just like the function of Photo-Coupler.

That's all of my question.Thanks a lot!

 

0 Likes
6 Replies
Anonymous
Not applicable

Hi Rickzhou,

   

 

   

PSoC 3/5 internal architecture has separate supply for Analog, Digital and I/O which are through the pins Vdda, Vddd and Vddio respectively. The 4 Quadrants of the Chip can be used with 4 different Vddio levels.

   

There are also 2 internal 1.8V regulators which provide the digital (Vccd) and analog (Vcca) supplies for the internal core logic.

   

More information on the power supply system can be found in the Technical Reference Manual at the following link:

   

http://www.cypress.com/?docID=26848

   

 

   

Also for optimum use of the Analog block, some Best Practises has to be followed, which are highlighted in these Application Notes:

   

http://www.cypress.com/?docID=25562

   

http://www.cypress.com/?docID=26389

   

 

   

Regards,

   

dasg

0 Likes
Anonymous
Not applicable

Dear Dasg

   

    Thanks a lot for your  great  help and the articles you show to me are very helpful! But should I ask something more about the analog interface,just like the picture attached?

   

     Because some analog components like ADC,DA and Comp will transfer some data to UDB or CPU through analog interface. And can the analog interface isolate analog and digital entirely,just like photo-couple? If it can't  the separation of power supply and GND may be meaningless in some strict conditions.

   

        Thank you very much!  

   

     Rick

 

0 Likes
Anonymous
Not applicable

dasg, can you provide updated links for that two application notes you mentioned? Thanks. Simon

0 Likes
ETRO_SSN583
Esteemed Contributor
0 Likes
ETRO_SSN583
Esteemed Contributor

True Galvanic isolation requires transformer, opto, RFID, various technologies to achieve
the isolation normally associated with Glavanic isolation. There have been manufactuers
that have done so thru hybrids and special die technologies, like Analog Devices –

   

http://www.analog.com/library/analogdialogue/archives/40-12/iso_power.html

       

But Galvanic does not imply isolations specs, so you have to look at what’s actually trying
to be achieved. Normally split busses between Analog and Digital do not imply Galvanic,
since the interface grounds ultimately meet.

   

Hope the info helps, regards, Dana.

0 Likes
HeLi_263931
Honored Contributor II

The iCoupler devices from Analog might be what you need. In the end, your solution would look like the original one you described (with the opto couplers) - the PSoC cannot replace true galvanic isolation. With the (e.g.) ADuM3000 devices, you can replace 4 opto couplers and can isolate a complete SPI interface.

0 Likes