Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Dear All,

   

I would like to get the ADC_SAR output register data connected directly to the output pins of PSoC5LP device. The datasheet indicates that "The CPU or DMA can access these registers to read the ADC result.". Do I have to use DMA to transfer the data to another register? I am trying to make a functional copy of old ADS7832 converter using PSoC5LP.

   

BR,

   

 

   

   Esa

0 Likes
5 Replies
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Some possibilities -

   

 

   

1) Using EOC output of A/D just trigger an ISR and in ISR write the result, byte wide, to

   

chosen port.

   

 

   

2) Use DMA, to SRAM. and ISR attached to nrq pin of DMA component. Then perform same

   

as 1) above.

   

 

   

3) Use DMA to SRAM, then use EMIF component. This is a bit of a guess, but possible

   

hardware only solution, you would have to investigate.

   

 

   

4) Use Verilog solution.

   

 

   

Regards, Dana.

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Or even simpler - just do a DMA directly to to output port. Place a register which functions as your port, and then do a peripheral-to-peripheral DMA. Look at AN52705 for an example (tough it uses tha DAC for that)

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Simplest would be 1), no additional HW used.

   

 

   

If control register placed, and A/D > 8 bits, takes 2 control registers.

   

 

   

Or DMA to the address of the port DR register(s).

   

 

   

Regards, Dana.

   

 

   

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

Using a control register allows to use non-adjacent pins (or pins from different ports). When writing directly to the DR, all pins must be of the same port.

0 Likes
ETRO_SSN583
Level 9
Level 9
250 likes received 100 sign-ins 5 likes given

Of course writing to non adjacent pins one has to use masking

   

for any other used pins in the ports being written to. But then that

   

is also true for use of full PORTXDR if ADC width does not match

   

port width and there are other used pins in port for other purposes.

   

 

   

Regards, Dana.

0 Likes