cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 5, 3 & 1

Anonymous
Not applicable

Hello i am trying to run a PWM module with a 48 Mhz clock frequency.

   

I am using the IMO; and i set the clock at 48 Mhz. This is not working, and i can only measure 3 Mhz with my oscilloscope. 

   

As the IMO is 3 Mhz, i figure that i need to do something else to get the 48 Mhz, described in this document:

   

http://www.cypress.com/file/140916/download

   

How can i get the 48 Mhz from the clock?

   

 

   

My project is attached. The clock i want to be 48 Mhz is the Clock_PWM.

   

 

   

Hope someone can help.

0 Likes
3 Replies
Bob_Marlowe
Expert II

Welcome in the forum.

   

You need to set the IMO to 48MHz. See your attached project archive.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thank you very much! It works exactly as it is supposed to.

0 Likes
Bob_Marlowe
Expert II

You are always welcome.

   

 

   

Bob

0 Likes