Announcements
Community Announcement : Welcome to the NEW Cypress Developer Community.
cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

ToIk_1341346
New Contributor

Do you have any garantee value of tensile strength at solder side?

MPN:CYBLE-022001-00

Regards,

Toshinari / TED

0 Likes
1 Solution
DavidS_06
Employee

Toshinari,

Tensile strength is not specifically tested on these products after mounting to a final product.  In general, a safe number would be 2kg horizontal tensile force after mounting onto the final PCBA.

Dave

View solution in original post

2 Replies
MichaelF_56
Moderator
Moderator

Moved both of your solder questions to the PSoC 4 BLE discussion forums so the applications team can review and provide a response.

0 Likes
DavidS_06
Employee

Toshinari,

Tensile strength is not specifically tested on these products after mounting to a final product.  In general, a safe number would be 2kg horizontal tensile force after mounting onto the final PCBA.

Dave

View solution in original post