cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hey Guy's

   

do i need an external programmer to program this kit?:http://be.farnell.com/cypress-semiconductor/cy8ckit-049-42xx/prototype-board-cy8c4245axi-483/dp/2420...

   

Whit best regards Ben

0 Likes
3 Replies
rola_264706
Honored Contributor II
        Well you can use a mini prog 3 or the bootloader host in Psoc Creator . Or another 049-42Xx their is an cypress document for it. Or you can use a 5lp kit as it has a programmer on it.   
0 Likes
Bob_Marlowe
Expert II

The CY8CKIT-049-42xx prototyping kit comes with a snap-off programmer that allows communication between PC and a Bootloader firmware within the PSoC4. Take the kit as it is named: a prototyping kit ready to build the core of a prototype. For development I would suggest you to get hands on a CY8CKIT-043 which allows for debugging and has a Kitprog which you might use to program any PSoC3 to 5.

   

 

   

Bob

0 Likes
rola_264706
Honored Contributor II

Here is the AP note to program the device with another device. http://www.cypress.com/knowledge-base-article/using-cy8ckit-049-program-another-psoc-4-kba93541?sour.... This is only necessary if your bootloader has been over written.  If you can afford it I would get this device as it is easier to use and you don't need to use the bootloader. CY8CKIT-043 PSoC® 4 M-Series Prototyping Kit. It contains the programmer and also has pads to add PSOC BLE module. 

0 Likes