network enable device via internet

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hello

   

Is it possible to control object (motor) using  Psoc4 kit via internet?

   

I mean can we connect Psoc4 kit directly to PC via internet to control the motor 

0 Likes
4 Replies
rola_264706
Level 8
Level 8
50 likes received 25 likes received 10 likes received
        Vead: yes there are Internet shields that plug into the the Pioneer shield connectors and there,are also motor control shields. Do a Internet search for 100 projects in 100 days there are two example projects in the list one for the Internet and one for the motor control. You could also do the control over the USB/serial kit prog interface and have a program on the PC that is connected to the Internet and decode the commands and send them to the PSOC 4 program.   
0 Likes
Anonymous
Not applicable

that means I need to purchase Internet shield.  I don't have internet shield

0 Likes
Anonymous
Not applicable

You could also do the control over the USB/serial kit prog interface and have a program on the PC that is connected to the Internet and decode the commands and send them to the PSOC 4 program.

   

How does PSoC4 get the commond from the PC that is connected to internet ?

0 Likes
EvPa_264126
Level 7
Level 7
500 replies posted 250 replies posted 100 likes received

Visit  http://www.e2forlife.com    page.
But, you might be interested in WiFi     ESP8266   module.
On the LUA language  firmware  nodemcu    this module solves these problems quickly and at virtually no cost.

0 Likes