PSoC™ 4 Forum Discussions
text.format{('custom.tabs.no.results')}
Hi,
I'm developing an application based on this UART TO BLE BRIDGE project:
http://www.cypress.com/blog/100-projects-100-days/project-020-uart-ble-bridge.
When data com from the UART interface, function CyBle_GattsNotification() is used to send data to the Central device.
For small frames ( tested with 15-16 bytes), it's works well.
For bigger frames ( tested with 24 bytes ), CyBle_GattsNotification() return an error ( CYBLE_ERROR_INVALID_PARAMETER ).
- My MTU is bigger than 24 ( actually 300 set on GAP settings , BLE component )
- Data characteristic size is bigger than 24 (30)
Do you have any idea about this problem ? Why i can't send more datas ?
Regards,
Thomas POINSOT,
ATEC Electronique
Show Less
yday i got a new prototype PSOC4200 board from cypress,pls explain me the steps where to start with and how to work on this board.
thanks in advance.
Show LessI have been trying for a while to find the GraphicLCDIntf component download specifically for the CY8CKit-041/2 boards but can only find the component available on the CY8CKit-059. Does this imply that the component cannot be used on PSoC4 devices? I note that in PSoc Creator 3.2 that the component will appear in the Catalog for the 059 but not the 042. If there is no underlying reason why the component will NOT work on the 042, how do I enable the component in the Catalog?
Thanks for your assistance.
Show LessIs it possible to have a constant password for BLE device ? If so how to do it ?
Following is th snippet of code where it generates Random 6 digit password and I want to make it contant.
What is the current consumption of low power comparator in deep sleep mode?
Dear,
I would like to check my HFCLK and put it in output.
How can I do this?
I connected an output to a clock but I have an error...
Thank you!
Show LessHi
I am trying to broadcast custom data for say 10 Sec and then go to deep sleep mode.
then Wake the after 8 Sec using WDT (counter 2) and then start broadcasting. continue doing the same forever.
but in the first time it broadcast for 10 sec. after timeout period. it go to Deepsleep mode. wakeup after 8 Sec( confirmed by toogling BLue LED in WDT ISR).
but does not Advertise furthur...
suggestions are most welcome.
i am attaching my project for Reference.
Thanks
Amol
Show LessHi,
Does anyone know how to use an EEPROM component with a PSOC 4M chip in Creator 3.2? I cannot find the component, and when I try to upgrade old designs that have one it says that it is incompatible, and does not try to upgrade to a new version.
Thank you,
Tom
I have placed SPIM master block in workspace then stop SPI block and went in deep sleep mode.
As per my understanding current should be 1-3 uA range but currently its 200 uA.
Please let me know how to fix this kind of problem.
I am facing same issue with ADC and Low power comparator.
Show Less