PSoC™ 4 Forum Discussions
I'm designing an app that connects to a sole Bonded device and while connected will broadcast a non-connectable, whitelist-only advertisement to up to 8 different devices.
Is the Bonded device stored in the same maximum-8 array, so that I would have to remove the bonded device address before populating the whitelist address?
If so, after removing the bonded address, populating the whitelist, advertising, and clearing the whitelist, how would I add the bonded device back to the bonded list for future connecting would StoreBondedDevices still apply and would/could I call it during connection or after disconnect?
I'm using component 3.10 and noticed in the docs that CyBle_GapRemoveDeviceFromWhiteList removes all devices, bonded and whitelist, but a parameter to allow them to be removed separately isn't available with this version. Is it a future release, or is it dependent on chip?
Thank you.
Show LessThe Module have a dedicated VREF pad, but I guess it's only for bypass cap use?
If I import a battery monitor example it wastes a pin, example P3.3 that it calls Vref.
What is the difference between VREF and Vref?
I have access to LDO 3.3V voltage, would this help getting around wasting a pin?
The 0.03Vdrop LDO is for a subsystem, so I do plan to run the BLE directly from li-po battery
and have it turn off the ldo when subsystem is sleeping.
Hello,
I use the device Cy8C4013LQI.
I must disable all components for power saving.
So I followed the instruction to change the debug interface to from SWD to GPIO.
Programming should always be possible.
But after download the firmware I can not connect the device anymore.
I use Segger-Jlink with the newest Firmware and software.
Here I found a similar problem.
http://forum.segger.com/index.php?page=Thread&threadID=2945
There are speaking about the version p, but in the download area only available version j.
So - how can I fix the problem? Now I blocked 3 prototypes.
Show LessHello,
I tried a lot of different things, but nothing works really good.
System-Resourcen
1 digital Input with pullup (used for WakeUp Key)
1 digital Output on 3.2 PWM mode strong drive
Clock 12MHz
If I try the following:
CySysWdtDisable();
PWM.Stop();
CyDelay(50u);
Motor_SetDriveMode(Motor_DM_ALG_HIZ);
Key_PWR_SetDriveMode(Key_PWR_DM_ALG_HIZ);
CySysPmDeepSleep();
still I consume aprox. 670µA on 3.3V
But only if I run this after a fresh Power-On Reset.
If I start the PWM, and run then in the same Power-Off, i come to 1.8mA
How can I save more Power? The Hibernate-Mode don´t exists on this device.
In the Datasheet should be the Power-cosum in DeepSleep 4.5µA - this would be nice.
What must I do, to save the maximum power as possible. I will wakeup on Key-IRQ, I must not keep nothing in Ram - I can reinitialize all again.
Show LessWill this also work for PSoC4 BLE devices?
I have customer server service, with one character as uint8[128].
I want to implement as when the client request a read request, the server will fillin new values, then return with new values.
So my question is the CYBLE_EVT_GATTS_READ_CHAR_VAL_ACCESS_REQ is invoked before send out the read response or after the read response?
Show LessHello,
I'm wondering if it is possible to modify the timeout interval between sending a Write Request (using CyBle_GattcWriteCharacteristicValue) and getting CYBLE_EVT_TIMEOUT event in case the Write Response is not received. The default timeout seems to be 30 seconds, which is a bit too long for our application. Changing cyBle_connectingTimeout has no effect (it works for connection timeout, though).
We are using CYBLE-022001-00 and BLE component v2.30 in PSoC Creator 3.3 CP2.
Thank you in advance!
BR - Stefano Voulaz
Hello,
My idea is to save whitelist data addresses in PRoC flash memory.
Is there in PRoC any component that emulates a EEPROM ?
Best regards,
Asier.
Show LessWith Wearable BLE, the design will pretty much be based around the coin-cell diameter.
So I recommend next Cypress BLE module will not need ground clearance, as that is hard to find on top of a coin-cell.
Johanson Technology 2450A 2.4 GHz Zero Clearance Antenna
http://www.mouser.com/new/Johanson/johanson-2450A-mini-chip-antenna/