PSoC™ 4 Forum Discussions
Hello,
In my application, I need to measure relative position between my device and 3rd party BLE device in one axis. I need to know if 3rd party device is on the left of my device or on the right. First solution that came to my mind is to use one BLE module with RF switch and 2 antennas. Then it is possible to measure RSSI on both antennas. This will tell if the device is closer or farther to/from each antenna. However, this add some complexity to the project (complex antenna tuning).
I wonder if I can use 2 BLE modules with built-in antennas and somehow coordinate them to do the job. Is it possible to simulate single BD_ADDR device using 2 actual modules? It would be nice to avoid double pairing with 2 modules. I would like to use one module as the master controller and another one as the radio frontend only.
Thank you for any suggestions.
Show LessHi All,
I am using KITPROG-043 and I have a UART component that prints DEBUG messages on Pins P7.0 and P7.1. As I have detached the KITPROG from PSoC4 I need to use the Pins provided on J2 header.
When I connect external FTDI to P7.0 and P7.1 I am not getting any debug messages. Is there some settings required for this? Can anyone help me with setting up UART DEBUG port?
Thanks in advance.
Lovelesh
Show LessDoes anyone know if it's possible to write programs for, and then program, the CY5670 BLE dongle in PSoC Creator?
From reading around I can see that's not the intended use but the CYBL10162-56LQXI is available in device selector and I'm thinking perhaps I can build the application and use PSoC Programmer to program the dongle maybe?
Show Lesswhen i try to put opamp and sar adc on schematic than i got this below message attached in image and i cant put component on schematic.
how can i resolve this error??
Show LessHi,
What is the correct Vcc value to be applied during programming of the IC via SWD?
We are using the MPQ 4-port programmer which requires the user to provide power to the IC. The programming spec document does not appear to contain this info.
Show Less
Hi
Please find attached coding. Iam unable to pair with my mobile. The kit is sending pass key but provision for entering the value in my mobile is not enabled.
my objective is to pair the PSOC module with my mobile using authentication and pass key.
Regards
Jagdish
I can not program the devices CY8CKIT-49-41xx and 49-42xxx, the message is "
01:50:46 PM - Communication port reported error 'Unable to read data from the target device'."
If I have previously programmed devices, but after the upgrade is impossible.
Nor do I appear ports in PSOC Programer and I deleted and reinstalled the driver devices.
Regards.
Show LessHello,
The cypress Proc4 BLE gives direct advertising report event, even when the direct address from the advertising device is not resolvable private address (Section 7.7.65.11, BLUETOOTH SPECIFICATION Version 4.2 [Vol 2, Part E]).
In detail:
I am using the CY5676A PRoC module in HCI mode, with the latest Bluetooth component(v3.10). The UART pins on the module receive/send the commands/events from/to a computer using script.
The advertising device has non-zero IRK and the scanning device has zero IRK, and the advertiser is set for direct advertising high duty cycle. The peer device is set for scanning with filter policy 2 or 3. What the script expects is a advertising report, while what the scanning device generates is a direct advertising report.
Anyone faced the same issue? Is there already a bug fix on this?
Regards,
Kiran
Show LessHi There,
The latest Cypress Product Roadmap shows that the CYBLE-214009-00 256KB EZ-BLE should be in production/available as of Q2 2016. We're in Q3 now and I've been waiting for this module to become available. (I know I can buy the EVAL board but that's an EVAL board!)
Does anyone know how long it is likely to be before I can order these new modules?
Thanks,
George