PSoC™ 4 Forum Discussions
I want to use the c# example to program psoc4 chip, the console example work, is it possible to get the miniprog3 state(connected or disconnected) using the reference PP_COM_WRAPPER? Or should I use openPort everytime when I execute program?
Show LessHi everyone,
I am developing small device with PSoC4 module. Next week the device is supposed to take certification test for wireless. Therefore I would like to have sample code for the below.
1. To transmit non-modulated continuous wave with fixed frequency
2. To change frequency
3. To transmit modulated continuous wave with fixed frequency
4. Receive mode
5. BLE test mode for checking with BLE tester
Best wishes,
RY
Hey folks,
I'm working with the CY5677 Dongle. I developed a custom application based on the Madhu Sudhan's example which can drive the Dongle to connect and drive a slave like CySmart permits to do. The dongle is programmed with the software used for CySmart. That's working very well.
I now have to develop a new application (or upgrade this one) which can read 2 slaves simultaneously, so here is my question : Can I make it with this configuration or the Dongle and the software on it will limit me to one slave ?
Regards,
Guillaume
Show LessHi,
I have an issue with the Device Address of my Sensors
I have configured the Public address (Company ID - Company assigned): with [3bytes]-XXXXXX and Silicon generated "Company assigned" part of device address Checked.
I thought that this identifier was unique, but now i have some duplicated Device Address in my Data Base.
How is possible??
How can solve this problem??
Thanks,
Sergio
Show LessHi,
I have a problem with using GPIO pins. If I have nothing connected to the pin that I want to use, then it works well (it changes its value from 0 to 1 and from 1 to 0 if I want to), but when I connected VCC pin from another device to that pin, then I can't change port's value from 0 to 1. The idea is to make this external device run once in a while, so I want to let's say set the pin to which the VCC is connected to 1 every 10 seconds, and after that change it to 0 so that this external device will not be working more. Could anyone help me with this? I set the pin to digital output with the Strong Drive mode and Initial state drive to 0. And I'm using Port 1.5 which is pin 42.
Show LessHello, I´ve read that the CY8CKIT-042-BLE can handle only 4 slave connections, I´wondering if it
is other chip of Cypress can handle the maximum slaves, 7 plus one master.
Thanks
Show LessHi I am using CYBL10573-56LQXI. I have setup an UART with the SCB and I want to change the baudrate when the device is running. I have read the specification explaining how to configure the clock divider to setup the target baudrate, but I do not quite understand.
To change the badrate dynamically, I know I need to use an external clock for the UART. By following the example in the spec:
// Target buadrate = 115200, over-sampling = 16, HFCLK = 48MHz
To set the frequency of the UART clock source: UART Clock = 115200 x 16 = 1.8432MHz (So I write this in to the Clock source of the UART)
Then Divider = HFCLK / Uart Clock = 48M / 1.8432M = 26
Then I start the clock and UART by this:
UART_Clock_SetDividerValue(26); // I found the API will subtract the parameter by 1, so I do not subtract myself
UART_Clock_Enable();
UART_1_Start();
However I cannot get it work. I found that if I set the divider to 25:
UART_Clock_SetDividerValue(25);
Then it will work. Why?
Also, in this way I can only change the divider number, which cannot let me to change the buadrate dynamically, how can I change the baudrate to for example 19200 when the device is running?
Thank you.
Show LessI need any example how work with Write Long Characteristic Value.
My device receive :
CYBLE_EVT_GATTS_WRITE_CMD_REQ
CYBLE_EVT_GATTS_PREP_WRITE_REQ
CYBLE_EVT_GATTS_EXEC_WRITE_REQ
What to do ? How response to this events ?
Show LessJeff.
Are there any iOS or Android tutorial videos or docs w/ example source for basic file transfers to a CYSPP based server?
Also, does Cypress plan to devote continued resources for providing support and 'timely' updates to CYSPP as inevitable bugs begin to appear in the field with any new host platforms? This seems like a daunting task not necessarily within the historical Cypress core product offerings.
Thanks for any business plans insight.
Show LessHello
I am trying to make a program to get temperature reading and send between two cy8ckit 042 ble kit. And want to see the results through UART.
Till now i tried UART_BLE example from https://github.com/cypresssemiconductorco/PSoC-4-BLE/tree/master/100_Projects_in_100_Days
Can anyone help me how to proceed from here??
Thanks
Show Less