PSoC™ 4

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
wangyuanfan
PSoC™ 4
I want to see what is ready to use with my dev-board. Regarding to section 3.4 "KitProg Driver Installation" (at KitProg User Guide (cypress.com) ), I... Show More
niharika
PSoC™ 4

can psoc6 be integrated with chip whisperer, if so please let me know how. 

Thanks 

s1m1ch
PSoC™ 4
Hi, because of supplier's stock shortages and too long lead time we are forced to replace the existing CY8C4247AZI-L423 MCU part number with CY8C4247A... Show More
saga_1136906
PSoC™ 4
Hi, I've a Cyble-012011-00 and I can't connect with a CYSMART 1.3. The log is: [11:04:46:581] : 'Resolve and Set Peer Device BD Address' request sent[... Show More
hesc_1314511
PSoC™ 4
Hallo, about CY8C4014PVI-42, has it ADC? I tried on Psoc creator, and a message say to me, I need to use the capsens, is it?thanks John Show More
wangyuanfan
PSoC™ 4
My dev-board is installed KitProg2 by default. I want to update the firmware from KitProg2 to KitProg3. Can I back-up default sipped state before upda... Show More
RideMaker
PSoC™ 4
I'm new to PSOC usage.  I have been assigned a completed project to update. It has been compiled for a CYBLE224110-00 MODULE, but I want build and upl... Show More
hoop4g
PSoC™ 4
Dear Team Cypress,Can CY8C4125PVE-S422 , together with Motor driver, control Stepper Motor through SPI communication for micro-stepping? Can CY8C4125P... Show More
AuKa_4634111
PSoC™ 4
I am trying to create a Monostable of 300mS than is triggered every second. It was easy enough when I worked with a 16 bit counter because a PWM count... Show More
JohnWinters
PSoC™ 4
I configure one discriptor for the DMA. It is set for 10 transfers. I do NOT configure it to invalidate the descriptor on completion.   10 triggers co... Show More
Board Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
Top liked authors