Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

PSoC™ 4 Forum Discussions

ToWa_1311181
PSoC™ 4
Hi, We use PSoC 4.2 BLE 256KB Module of CY8CKIT-143A as daughter board to build our hardware prototype. The hardware prototype isfunctional. And then ... Show More
RoCa_1222471
PSoC™ 4
I'm using a CY8C4248LTI-L485 device and I'm observing a +/-2% clock acccuracy for IMO clock. Is it possible to trim this clock during production (usin... Show More
MKN_4249821
PSoC™ 4
Hi all,I am trying out the example of FixedStack OTA bootloading for PSoC 4 BLE device. I am doing the steps as described but I got error in step 11. ... Show More
mata_3748076
PSoC™ 4
Is there any sample code for CAN interfacing available for PSOC 4100 s plus (CY8CKIT-149)amily microcontroller?Please provide links. Show More
DaYe_3972766
PSoC™ 4
Hi All,Running on CY8C4247AZI-M485,I have an application (bootable) and a bootloader.I followed instruction in "Emulated eeprom v2.0" and got everythi... Show More
JoWi_3984961
PSoC™ 4
After getting told my 8051 license had run out (I thought I was using ARM in the PS0C so I ignored that), all my preferences, links to my projects, et... Show More
maze_1672671
PSoC™ 4
Hello all,my colleagues in the test department found a flash corruption caseOur device is connected to the battery of cars, so it is powered at 12 V; ... Show More
EyGe_3183606
PSoC™ 4
Hello,We print constantly the Gatt error code to UART for debugging purposes.Recently we encountered a case where the value was 2000171b (it was print... Show More
kalac_4244351
PSoC™ 4
Newb here.  I’m trying to find more details on this device, like the accuracy/stability of the 32.768 kHz xtal (I’m considering the board for a time k... Show More
Dave_Long
PSoC™ 4
Hi ALL:  What's the AD value when a pin of the MCU was set to a AD function but connect nothing for Psoc S2? Show More
Forum Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy