PSoC™ 4 Forum Discussions
Hi I have a capsense project working on PSOC 4200M and I have used the example code. Now I want to make the code work as an interrupt so that I can run a program in my main for loop and change modes when the capsense triggers. I have no idea how to do that. Can anyone help with example code?
Show LessReading from raspberry pi via I2C - how can I reset the read pointer to the first byte of the read buffer by my raspberry? I am using python on the raspberry.
Show LessI’m Giovanni Bengalis, I’m a Firmware Engineer Junior,
I have an internal project which is a bit complicated for me. I want to create a fake rotary (fixed) with Capsenses on the vertical walls (attachment)
The rotary switch can be used by a left-handed or a right-handed, I proposed a linear slider on 75% of the circle, with this slider I would capture the position when the first touch and compare it with the last position captured when the Capsense would be released.
However, the bad news was the library Capsense can not handle more one finger at the same time.
So I contact the community to know if there is a solution to handle more one finger at the same time because the pro of the linear slider is to return the position of the finger and with the position I'll determine the direction of the rotation.
I am open for any other ideas to success this project.
Thank you for your help,
Show LessHi Friends,
I need to add a variable in Generated Source Files (in FIleName_UART.c & FileName_SPI_UART.h) every time.
If I clean & rebuild my project or restart PSoC Creator, then these modified files are overlapped by newly generated ones.
How can I solve my problem?
-Chinmay
Show LessHello,
(1) I2C communication buffer size in Bootloader
Users are creating a Bootloader with an I2C interface to update PSoC Firmware via an external MCU. Firmware update has been confirmed to work properly. At this time, in Bootloader_Start (), a fixed-size buffer of 64 bytes is allocated as the I2C communication buffer.
Is it possible for the user to change the Bootloader I2C buffer size? (Size larger than 128 bytes)
I found I2C buffer size definition in I2C_Slave_BOOT.h.
#define I2C_Slave_I2C_BTLDR_SIZEOF_READ_BUFFER (64u)
#define I2C_Slave_I2C_BTLDR_SIZEOF_WRITE_BUFFER (64u)
(2) About obtaining bootloader version information
As a method to get the metadata (Appllication version, Application ID, Application custom ID) of the Bootloader component, the customer can get the value by executing the Get Metadata (0x3C) command of Bootloader Commands while entering Bootloader.
Is it possible to get these meta data from the Bootloadable project?
The customer wants to get these metadata information from the host MCU after Bootloadable_Load.
Best Regards,
Naoaki Morimoto
Show LessHello Cypress.
Q1)
When Tx clock source setting is “Auto”, how does CSX select it?
Below is my understanding.
Is my understanding correct?
====================================================
1: Check whether both of following 2 relational formulas are satisfied.
a) 20 =< ModCLK/TxCLK =< 160
b) Nsub >= (2^sscn-1) * (ModCLK/TxCLK)
2: The Priority order is as follows.
(Higher) SSC10 -> SSC9 -> SSC7 -> SSC6 -> Direct (Lower)
(TX clock source setting becomes “Direct” if either a) or b) of above formulas is not satisfied.)
====================================================
Q2)
If Q1 is yes, Number of subconversion needs to be quite large value in order for SSC to be selected.
In actual application, I think that SSC almost is not selected.
Even if CSX Tx clock source setting is “Auto”, sense clock source will become “Direct” in most cases.
Is my understanding correct?
For example, if ModCLK is 24000kHz and TxCLK is 300kHz, SSCx is not selected regardless of value of subconversion.
SSC is difficult to choose, so CSX noise tolerance seems to be worse compared to CSD.
CSD’s SSC is also difficult to choose, but CSD has PRS.
Please advise it.
Do you have any information and comment about it?
Best Regards.
Yutaka Matsubara
Show LessI'm trying to make a luxometer using PSOC 5LP CY8C5888LTI-LP097 with this code
#include <project.h>
#include <stdio.h>
#include <math.h>
int main()
{
uint8 i;
int Lux;
LCD_Start();
char8 publicar1 [22];
float32 conversion1,conversion2;
CyGlobalIntEnable;
ADC1_Start();
ADC1_StartConvert();
ADC1_IsEndConversion(ADC1_WAIT_FOR_RESULT);
for(;;)
{
LCD_PrintString("Int.Luminosa");
LCD_Position(1,8);
conversion1 = ADC1_GetResult16(0);
conversion2 = ((5.000000*conversion1)/1024)*0.232;
Lux = ((2500/conversion2)-500)/5;
LCD_PrintString("Lux");
LCD_PrintNumber(Lux);
LCD_Position(0,2);
CyDelay(200);
if(Lux>=51 && Lux <=200)
{
for(i=0;i<30;i+=2)
{
LCD_DrawHorizontalBG(1,0,2,i);
CyDelay(150);
}
LCD_ClearDisplay();
}
if(Lux>=202 && Lux <=350)
{
for(i=0;i<30;i+=2)
{LCD_DrawHorizontalBG(1,0,3,i);
CyDelay(150);
}
LCD_ClearDisplay();
}
if(Lux>=360 && Lux <=600)
{
for(i=0;i<30;i+=2)
{LCD_DrawHorizontalBG(1,0,4,i);
CyDelay(150);
}
LCD_ClearDisplay();
}
if(Lux>=620)
{
for(i=0;i<30;i+=2)
{LCD_DrawHorizontalBG(1,0,5,i);
CyDelay(150);
}
LCD_ClearDisplay();
}
}
}
and this is the diagram for the protoboard
and the ports P2[6:0] and P0[6]
please help
Show Less