PSoC™ 4

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
JohnWinters
PSoC™ 4
I configure one discriptor for the DMA. It is set for 10 transfers. I do NOT configure it to invalidate the descriptor on completion.   10 triggers co... Show More
KiSm_967071
PSoC™ 4
I am upgrading a design from using the Cy8C4246AZI to the Cy8C4248LQI-BL573 or BL583.  In my Cy8C4246 design I have an IR receiver module connected to... Show More
AuKa_4634111
PSoC™ 4
I am trying to create a Monostable of 300mS than is triggered every second. It was easy enough when I worked with a 16 bit counter because a PWM count... Show More
YSJE_3566666
PSoC™ 4
Dears. Is there a way to program a hex file without PC or laptop when using the miniprog3/4? We need a simple programming method by connecting power t... Show More
hesc_1314511
PSoC™ 4
Hallo, about CY8C4014PVI-42, has it ADC? I tried on Psoc creator, and a message say to me, I need to use the capsens, is it?thanks John Show More
Renate
PSoC™ 4
The CYBLE-012011 BLE modules uses digitally tuned trimmer caps on the xtal to be on frequency. The example projects leave you with values of 0x2d6a (8... Show More
RideMaker
PSoC™ 4
I'm picking up a project and haven't used the Cypress PSOC parts before.  I have two board variants with two different PSOC 4 BLE parts in them: CYBLE... Show More
hoop4g
PSoC™ 4
Dear Team Cypress,Can CY8C4125PVE-S422 , together with Motor driver, control Stepper Motor through SPI communication for micro-stepping? Can CY8C4125P... Show More
patrick1957
PSoC™ 4
Hi, I'm using "CY8CKIT-145-40XX PSoC® 4000S CapSense Prototyping Kit" for evaluating CapSense capability.  It's working fine with code example "CE2107... Show More
Anonymous
PSoC™ 4
Hi,     I am trying to locate the source code for BLE Beacon Android app. Has anyone worked with it?Thanks, Show More
Board Information

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
Top liked authors