cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

ToIk_1341346
New Contributor

Do you have any criteria of visual inspection when module mounted to customer's board?

For example, compliant CP** etc.

MPN:CYBLE-022001-00

Regards,

0 Likes
1 Solution
DavidS_06
Employee

user_482230132,

The visual inspection criteria that we use in our factory is IPC 610 Class 2 for consumer electronic devices.  This may be used as well when the module is mounted to the end application board. 


Dave

View solution in original post

0 Likes
1 Reply
DavidS_06
Employee

user_482230132,

The visual inspection criteria that we use in our factory is IPC 610 Class 2 for consumer electronic devices.  This may be used as well when the module is mounted to the end application board. 


Dave

View solution in original post

0 Likes