Where is KitProg driver of  CY8CKIT-046 PSOC4 L-series Pioneer Kit??
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
Funny development kit...

   

I don't find any KitProg driver to use, how to fix it?

   

Thanks a lot.

0 Likes
10 Replies
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

It should be part of the Creator install (or maybe PSoC Programmer).

0 Likes
Anonymous
Not applicable

I already install anything (complete installation) with DVD ISO.

   

I can use CY8CKIT-042-BLE-A Bluetooth® Low Energy 4.2 Compliant Pioneer Kit as before with the installation.

   

So it is very strange....

   

Is there a way to restore KitProg of the board? I think that the KitProg maybe corrupt....

   

 

   

After restoring KitProg, it still no driver associates with KitProg...

   

I notice that my another computer(WIN10 64Bit) can detect driver and install, how to fix in WIN7 64Bit?

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Try to update the Kitprog as shown in the manual using PSoC Programmer 3.25

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hi,Bob

   

I already restore KitProg many times by using PSoC Programmer 3.25..., the result is the same.

   

Computer1(WIN7 64Bit)

   

CY8CKIT-042-BLE...OK

   

CY8CKIT-046...Not OK

   

 

   

Computer2(WIN10 64Bit)

   

CY8CKIT-042-BLE...OK

   

CY8CKIT-046...OK

0 Likes
rola_264706
Level 8
Level 8
50 likes received 25 likes received 10 likes received

Hold down the Reset button for 10 Sec and see if that helps.

0 Likes
rola_264706
Level 8
Level 8
50 likes received 25 likes received 10 likes received

Drivers for Kit prog are in the kit prog dir.

0 Likes
Anonymous
Not applicable

Hi, I already restore KitProg of the board and reinstall the driver many times...

   

But ONLY the CY8CKIT-042 Kit can be properly detected and installed driver.

   

CY8CKIT-046 is still not working...

0 Likes
rola_264706
Level 8
Level 8
50 likes received 25 likes received 10 likes received
        Have you re-installed the Psoc Creator on the windows 7 machine. That should reinstall all of the software. If it fails to work the I would say that there is some kind of software issue with the windows 7 machine as it works on the windows 10 system.   
0 Likes
Anonymous
Not applicable

I reinstall PSOC Creator 3.3 and 4.0, WIN7 machine doesn't show any errors and problems.

   

By the way, CY8CKIT-046 Mouse Demo (J11 USB Port) is also no driver to use, but WIN10 machine can properly install driver to use.

   

 

   

WIN7-CY8CKIT-042

   

.

   

WIN7-CY8CKIT-046

   

   

WIN7-CY8CKIT-046-DEMO

   

   

WIN10-CY8CKIT-042

   

   

WIN10-CY8CKIT-046

   

   

Thanks

   

   

   

   

   

0 Likes
Anonymous
Not applicable

Solve problem by upgrading WIN7 with Original DVD.

0 Likes