What is the maximum voltage differential between VDDA, VDDD and VDDR on the CY8C4248LQI-BL483

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

We have a design where there are beads feeding each of the supplies from a signal switching regulator (buck). For a particular customer we need to power several bright LED's from the VDDD bead because there is no connector on the board that has the direct regulator output. This will cause additional drop across the VDDD bead when the LED's turn on, so VDDD will be at a slightly lower voltage than VDDA and VDDR. What is the maximum voltage differential between the three supplies? We have a nominal 3.3 volt supply so is the differential basically the drop to the dropout level of the internal on-chip regulators?

Blair

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

VDDA must be the highest voltage and be less than 5V, 3.3V is ok..

VDDD must be greater 1.8V.

When VDDD changes some analog components as capsense, ADC, DAC or comparators might fail or deliver strange results.

Bob

View solution in original post

0 Likes
1 Reply
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

VDDA must be the highest voltage and be less than 5V, 3.3V is ok..

VDDD must be greater 1.8V.

When VDDD changes some analog components as capsense, ADC, DAC or comparators might fail or deliver strange results.

Bob

0 Likes