cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hi all,

   

I am having a very strange problem with UART communication, and I have spent a lot of time trying to find a reason for it. I am using the UART component (v2.5 and PSoC Creator 3.2) in full duplex, with flow control enabled and only the 4 byte hw buffer.

   

I have just made a new batch of my pcb and none of them are doing what they are supposed to do. Fortunately I had 2 older PSoC4's laying around for an older prototype, and mounting them on the PCB works just fine. There naming is "CY8C4245AXI-483 1431 A 04" and the none working units have "CY8C4245AXI-483 1525 C 32".

   

Anyone of you had similar problems? any critical silicon change that im unaware of? I know this is a risky judgment, but it is currently where I am, my design is pretty mature. 

   

It is like the UART hw buffers simply is not working the same way anymore. If I enable software buffer I see better behavior, but it is not an option for me right now. And I would like an explanation for this phenomenon.

   

Thanks in advance.

   

Regards

   

Dennis

0 Likes
1 Reply
ETRO_SSN583
Esteemed Contributor

I recommend you file a CASE right away on this -

   

 

   

To create a technical or issue case at Cypress -

   

 

   

www.cypress.com

   

“Support”

   

“Technical Support”

   

“Create a Case”

   

 

   

You have to be registered on Cypress web site first.

   

 

   

Regards, Dana.

0 Likes