Tuner GUI Connection fails PSOC4248AZI-L485

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

   

I have looked through some similar threads but I haven't come to a solution so far.

   

I am using a custom PSOC4248AZI-L485 Board and I cannot launch the tuner.

   

I have configured the EZI2C according to the settings using the pins P3_0/P3_1 , but when using the MiniProg3 the connection always fails.

   

Any clue what I am doing wrong?

   

Programming the device works fine.

0 Likes
2 Replies
Anonymous
Not applicable

Hello,

   

Have you checked the settings in both EZI2C components and tuner I2C parameters are same? Please verify if the I2C speed, I2C address in EZI2C component and tuner are same or not? Can you please attach the snap shot of the error. Please check with I2C speed of 100kHz and check if it is working. 

   

Thanks

   

Ramesh B

0 Likes
Anonymous
Not applicable

Hi Ramesh,

   

I have finally connected the board to Tuner GUI using the same settings but Port Pins P4.0 and P4.1 as the EZI2C component.

   

Kind of surprises me as the manual recommends using Pins 3.0 and P3.1. But finally it works.

   

Thanks for your thoughts and help.

0 Likes