I use a KitProg2 and KitProg3 programmers to program BLE modules, and that BLE capsense mouse: The programming hardware connector on the end device (mouse or BLE module has this connection)
My Question is: Is there any signals connected to pin 6 and pin 8 inside the programmer? I want to tie my Debug UART_RX and UART_TX back to these pins on my end application hardware so I have a one connector interface (my target hardware is potted for industrial use so I only want one connector) I can not find any documentation on the MiniProg3 at the hardware circuit level. just user manuals on how to configure an use the programmer. I dont want to sizzle the programmer or sizzle my end hardware if I tied the uart back to pin6 and pin8.
Solved! Go to Solution.
If you are going to use the SWD debugging with the Miniprog3, then you won't be able to use pin 6 for the UART. If you don't care about SWD debugging, then you can probably get away with using the pins 6 and 8 for the UART output/input.
I've been able to run/test my own miniprog3 debugging using only the 5-pin assignment for SWD, so you you won't need the SWV pin unless you want the extra debug functionality and decide to use the 10-pin connection.
I may have just found the answer: In MiniProg3 manual there is this drawing:
So this tells me MAYBE there is a problem? If I only use SWD on the programmer and do not switch it to JTAG then probably it is OK to tied my debug uart to pin 6 and pin 8. and it appears that pin 6 is SWV or the debug uart so I need to connect my UART_TX to pin6 and UART_RX to pin8 ????
If you are going to use the SWD debugging with the Miniprog3, then you won't be able to use pin 6 for the UART. If you don't care about SWD debugging, then you can probably get away with using the pins 6 and 8 for the UART output/input.
I've been able to run/test my own miniprog3 debugging using only the 5-pin assignment for SWD, so you you won't need the SWV pin unless you want the extra debug functionality and decide to use the 10-pin connection.