- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Has anyone had any success using the SI Labs Temperature and Humidity Sensors?
I am unable to read the sensor reliably. There is a CRC check function that is validating the 1st, 3rd and 5th reads when I have a CyDelay(1), but nothing else. Without the delay (as shown below) the first read is valid, but no others. I have tried changing the delays up to 1000 with no difference.
<code>
float SI7013_readHumidity(void)
{
//Request a humidity reading
I2C_1_I2CMasterSendStart(SI7013_ADDRESS, I2C_WRITE);
I2C_1_I2CMasterWriteByte(MEASURE_RH_NOHOLD); // Register to write at.
I2C_1_I2CMasterSendStop();
//Hang out while measurement is taken.
CyDelay(130);
uint8 msb, lsb, checksum;
I2C_1_I2CMasterSendStart(SI7013_ADDRESS, I2C_READ);
msb = I2C_1_I2CMasterReadByte(I2C_1_I2C_ACK_DATA);
//CyDelay(1);
lsb = I2C_1_I2CMasterReadByte(I2C_1_I2C_ACK_DATA);
//CyDelay(1);
checksum = I2C_1_I2CMasterReadByte(I2C_1_I2C_ACK_DATA);
//CyDelay(5);
I2C_1_I2CMasterSendStop();
//CyDelay(5);
uint16 rawHumidity = ((unsigned int) msb << 😎 | (unsigned int) lsb;
if(SI7013_check_crc(rawHumidity, checksum) != 0) return(999); //Error out
//sensorStatus = rawHumidity & 0x0003; //Grab only the right two bits
rawHumidity &= 0xFFFC; //Zero out the status bits but keep them in place
//Given the raw humidity data, calculate the actual relative humidity
float tempRH = rawHumidity / (float)65536; //2^16 = 65536
float rh = -6 + (125 * tempRH); //From page 14
return(rh);
}
</code>
I am hoping that I am just doing something stupid here.
Parts are on a custom PCB. I2C traces are VERY close to matched. I am using the original library on an arduino connected to the sensor via a cable and it works fine. So it isn't the sensor.
I have attached the Project. I am using Creator 4.1 Update 1.
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
Thanks Bob! Your code works very well.
I also got the following code to work:
I2C_1_I2CMasterSendStart(SI7013_ADDRESS, I2C_WRITE);
I2C_1_I2CMasterWriteByte(MEASURE_RH_NOHOLD); // Register to write at.
I2C_1_I2CMasterSendStop();
//Hang out while measurement is taken.
CyDelay(60);
uint8 msb, lsb, checksum;
uint8 buffer[3];
(void) I2C_1_I2CMasterReadBuf(SI7013_ADDRESS, buffer, 3, I2C_1_I2C_MODE_COMPLETE_XFER);
while (0u == (I2C_1_I2CMasterStatus() & I2C_1_I2C_MSTAT_RD_CMPLT)) { }
msb = buffer[0];
lsb = buffer[1];
checksum = buffer[2];
Not as eligant as yours, but it did work!
Thanks again!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content