- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hey all,
I'm Using the CY8CKIT-041-41XX PSoC 4100S touchpad and I have a problem with the sensor-Status getting stuck, if I touch the Sensor for to long.
And also if I use HF nearby, the sensor status sometimes doesn't return to zero or it takes a long time. I think it's because the rawcounts are still a lot higher than baseline.
So with no touch the values (Graph view, SenseTuner) are:
raw count: 54,430 -54,390
baseline: 54,390
after touch:
rawcount: 54,580-54,720
baseline: 54,415
(My widgit threshold Parameters are: FT:110; NT: 60; NNT:60; Low baseline reset:255, Hysteresis: 5, On debounce: 2, I use the 5x5 centroid type and activated the Jitter Filter. Also I tried it with the IIR Filter)
Do you know which settings I have to change, so the sensor status returns to zero right after unhanding the sensor?
Thanks in advance,
len
Solved! Go to Solution.
- Labels:
-
ispn:39610:1:0
-
l1:314:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello leko_4405711
In the configure CapSense window, under the Advanced tab, there is an option for "Enable sensor auto-reset". Please select this option and it will cause the baseline to be updated always.
Please note that long press will not work if this feature is enabled since the baseline tracks raw counts.
Thanks and regards
Harigovind
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello leko_4405711
In the configure CapSense window, under the Advanced tab, there is an option for "Enable sensor auto-reset". Please select this option and it will cause the baseline to be updated always.
Please note that long press will not work if this feature is enabled since the baseline tracks raw counts.
Thanks and regards
Harigovind