Dear Sirs,

   

I'll be very grateful if you could review my schematic for the communication between the host uC and the BTLE module CYBLE-022001-00: I wasn't be able to find the related documentation while in a detailed AN for microchip BTLE module RN4020 I've found the necessary signal lines.

   

The purpose of the application is to communicate with a heart rate chest strap and a smartphone. I think to an UART communication between the host uC and the BTLE module.

   

Moreover I'd like to use 3 leds for connection status.

   

Thank you in advance

   

Andrea

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Since you did not provide us with the complete project there is a bit of guessing to answer your question.

   

First: The 4200 BLE  UART (SCB) does not provide hardware handshake using CTS and RTS. You will need to use the UDB-based version (v 2.50) to perform that.

   

 

   

We cannot check if your pin-assignments are ok, so best will be to post your complete project, so that we all can have a look at all of your settings To do so, use
Creator->File->Create Workspace Bundle (minimal)
and attach the resulting file.



Bob
 

0 Likes
lock attach
Attachments are accessible only for community members.
Anonymous
Not applicable

 Please,

   

find in attachment the project. It seems that the RTS and CTS are managed!

   

BR

   

Andrea

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Andrea

   

That looks good from the PSoC side. Check the following:

   

You have an interrupt firing 1000 times per second, that is much, do you really need that frequency?

   

There already is a 32,768Hz clock, you may save another clock running at 32.000Hz (saving some power)

   

Hardware handshake looks OK.

   

Have you already got an evaluation board to check your design?

   

 

   

Bob

0 Likes