cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

HeGi_2497906
Contributor II

I have run out of ideas on why my SPI is not working, just will not function, I have tried so many ideas, none seems to work.

In the code attached, I am simply trying to read the ID register address 0x00 which should read 0x20, all I get is 0xFF.  This device has an ID register, and the EE_READ_ID function is supposed to just read that value for now.

I could really use some help, any suggestions would be appreciated.  I reviewed the SPI Master example and coded my SUBR ST_EE_PROM.C based on the instructions.  I just do not see why it will not read the register.

Herb

0 Likes
1 Solution
Anonymous
Not applicable

I see that you are using the wrong API function. As I mentioned in the previous post, you need to use SPIM_SpiUartGetRxBufferSize(); instead TX buffer size is being read.

-Rajiv

View solution in original post

0 Likes
10 Replies
Anonymous
Not applicable

Herb,

You need to wait for 4 bytes to be sent before reading the ID from the FIFO. Please use the below code after SPI_SpiUartPutArray(EE_TX_buf,4) function call-

while(SPIM_SpiUartGetRxBufferSize() != 4);

  

SPI_SpiUartPutArray() function waits only if the TX buffer is not empty; otherwise, it simply loads the data into the buffer and returns.

-Rajiv

0 Likes
HeGi_2497906
Contributor II

Well that did not work, so please remove the correct answer, all that did was make the code halt there and reset, nothing is being sent, no data, SS or clock.

Here is the modified code, this is becoming and urgent problem, this should be working.

Herb

0 Likes
HeGi_2497906
Contributor II

We may have found a hardware connection issue, that was not on the test board.  If so, it would explain why things were not working.

0 Likes
Anonymous
Not applicable

Good to know. But note that you still need to wait for the data to be sent completely before reading the RX buffer. The code should not have hung up at the while loop; need to see if there is something else causing the problem. Let us know the result after fixing the hardware connection issue which you mentioned.

0 Likes
HeGi_2497906
Contributor II

The hardware issue was not correct, the device is wired correctly, the pins are assigned correctly.

Still does not work, and hangs on the buffer check line until it resets.  If I comment out that line, it does not reset.

Also, I my BLE will now not show up advertising, I checked the instruction with the debugger and it execute the Stack on and the Start_Advertising, but nothing on the scanners.

Rest of the functional code that controls the outputs works?  Does not appears to be resetting.

Please take a closer look?  I really need the help to get over these concerns.

Herb

0 Likes
HeGi_2497906
Contributor II

The while loop is blocking and my WDT interrupt was crushed by it, so it crashed.  I added a CY_Delay(10); into my EE code and it all works now.

Is there a code function that will wait but allow interrupts?

0 Likes
Anonymous
Not applicable

I see that you are using the wrong API function. As I mentioned in the previous post, you need to use SPIM_SpiUartGetRxBufferSize(); instead TX buffer size is being read.

-Rajiv

View solution in original post

0 Likes
HeGi_2497906
Contributor II

Thank you Rajiv, as we all get there when coding, you cannot see the problem right in front of you.

And for those who may need it, here is a working, Write Enable, Checks the Write Enable bit, Writes, Reads and compares a single byte to any address in an EEprom.  Below is the Read function.

/*******************************************************************************

* Function Name: Write a memory location

********************************************************************************

* Summary:

*   Write a particular memory location, defined by High Byte, Low Byte

*   The read it back to make sure it was written

* Parameters: 

*   Up to 11 bits of addressability 0b (XXXX a11a10a9a8a) (7a6a5a4a 3a2a1a0)

*

* Return:

*   if successful, the data word is returned

*   if unsuccessful EE_WRITE_ERROR constant is returned

*******************************************************************************/

uint8 EE_Write_Addr(uint8 HighByte, uint8 LowByte, uint8 data)

{   

    SPI_SpiUartClearRxBuffer();

    SPI_SpiUartClearTxBuffer();

    // Send the wrtie enable command

    SPI_SpiUartWriteTxData(EE_WRITE_ENABLE);

   

    while(SPI_SpiUartGetRxBufferSize() != 1);

    SPI_SpiUartClearRxBuffer();

    SPI_SpiUartClearTxBuffer();

    // build the output buffer to read the status

    EE_TX_buf[0] = EE_READ_STATUS; // read status instruction

    EE_TX_buf[1] = EE_PAD_BYTE; // pad one for status word

    EE_TX_buf[2] = EE_PAD_BYTE; // pad two for status word

    // write the buffer

    SPI_SpiUartPutArray(EE_TX_buf,3);

   

    while(SPI_SpiUartGetRxBufferSize() != 3);

   

    // read the buffer

    EE_dummy_read = SPI_SpiUartReadRxData();

    EE_RX_buf[0] = SPI_SpiUartReadRxData();

    // test for write enable bit

    if(EE_RX_buf[0] != EE_WEL_BIT)

      {  

        ID_Value = EE_WREN_NOT_OK;

            return ID_Value;

      }

   

    // WREN is good so write the byte

    EE_Adr_high_byte = HighByte;

    EE_Adr_low_byte = LowByte;

   

    // build the output buffer

    EE_TX_buf[0] = EE_WRITE; // write instruction

    EE_TX_buf[1] = EE_Adr_high_byte; // High byte

    EE_TX_buf[2] = EE_Adr_low_byte; // Low byte

    EE_TX_buf[3] = data; // data for writing

    SPI_SpiUartPutArray(EE_TX_buf,4);

   

    while(SPI_SpiUartGetRxBufferSize() != 4);

  

    // Read the address

    EE_Read_Addr(HighByte,LowByte);  // returns READ_Value

   

    // Test it against data to ensure it was written correctly

    if(data != READ_Value)

    {

        return EE_WRITE_ERROR; // if no match signal an error

    }

    return READ_Value; // if a match return the value

   }

/*******************************************************************************

* Function Name: Read a memory location

********************************************************************************

* Summary:

*   Read a particular memory location, defined by High Byte, Low Byte

*   

* Parameters: 

*   Up to 11 bits of addressability 0b (XXXX a11a10a9a8a) (7a6a5a4a 3a2a1a0)

*

* Return:

*   READ_Value value at that address

*  

*******************************************************************************/

uint8 EE_Read_Addr(uint8 HighByte, uint8 LowByte)

{   

    SPI_SpiUartClearRxBuffer();

    SPI_SpiUartClearTxBuffer();

    EE_Adr_high_byte = HighByte;

    EE_Adr_low_byte = LowByte;

   

    // build the output buffer

    EE_TX_buf[0] = EE_READ; // read the ID instruction

    EE_TX_buf[1] = EE_Adr_high_byte; // High byte

    EE_TX_buf[2] = EE_Adr_low_byte; // Low byte

    EE_TX_buf[3] = EE_PAD_BYTE; // pad for data collection

    SPI_SpiUartPutArray(EE_TX_buf,4);

    while(SPI_SpiUartGetRxBufferSize() != 4);

   

    EE_dummy_read = SPI_SpiUartReadRxData();

    EE_dummy_read = SPI_SpiUartReadRxData();

    EE_dummy_read = SPI_SpiUartReadRxData();

    EE_RX_buf[0] = SPI_SpiUartReadRxData();

    READ_Value = EE_RX_buf[0];

   

    return READ_Value;

}

0 Likes
Anonymous
Not applicable

You're welcome Herb. I too missed seeing the error in the edited code in the first reading.

Also, thanks for putting the code. It will definitely help others. Can you please let us know the code example you referred? I will check if it requires any improvement.

- Rajiv

0 Likes
HeGi_2497906
Contributor II

The SPI master, I get it now, but it was hard to follow.

Also, I have another request in the system on Apple phones losing BT connection in 30 seconds, Android stays connected, please look into that one ASAP.

Herb

0 Likes