cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

HuEl_264296
New Contributor II

Is it possible to run an SCB UART at 3Mbaud?

   

According to the datasheet, the max speed is 1Mbaud. But if I connect an external 24MHz clock, and set the oversampling to 8x, that should give 3Mbaud.  When I do this, I don't get any compiler errors or warnings.

   

Is this likely to work?

   

Hugo

0 Likes
2 Replies
odissey1
Honored Contributor II
0 Likes
HuEl_264296
New Contributor II

Hmm. It doesn't explicitly mention 3Mbaud, but it does mention 2Mbaud, which is higher than  the datasheet claims.

   

I guess I'll just have to try it.

   

Hugo

0 Likes