Report Map sharing

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

   

I wrote application over HOG. Connection is successful. But I am seeing that Connection time is arounf 11-12 seconds while with the standard application give, I am seeing this connection is happening in 3 seconds.

   

Please Let me know, if anything I need to look into.

   

ManyThank ...

0 Likes
3 Replies
Anonymous
Not applicable

Can you share your project? As I understand, it takes longer time to get connected. What is the advertisement interval? Are you using fast advertisement?

0 Likes
Anonymous
Not applicable

Hi Thanks for the reply. 

   

Yes, I am using fast advertisement 

   

below are the parameters I have set. 

   

fast advertizing interval  min  = 60ms

   

​fast advertizing interval  max  = 60ms

   

​Slow advertizing time out =  30 s 

   

Fast connection advertizement time out =  30 s

   

Slave lateny 4 

   

Pref max conn. int =  0x 000a

   

Pref min conn. int =  0x 000a

   

​Supervision timeout = 0x 0018 

   

These the time params i have set.  please let me know if any one to be tuned or any param is missed by me. 

   

Related to your Question about sharing the project: I am really sorry, my proj manager did not allow me. 

   

Looking forward for your response. 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

You may create a support case to get in contact with Cypress directly. They will keep all information confidentially, none of your information will be presented to any users. Use at top of this page "Design Support".

   

 

   

Bob

0 Likes