cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

David_Zhang
New Contributor II

   When i use the CY8CKIT-042 PSoC® 4 Pioneer Kit , it can download and debugger, but it can't connect to Launch Tuner, it shows tha read  operatuon failed ! check I2C bus connection, the confiration is following below;

pastedImage_0.png

pastedImage_1.png

the project has been attched, please help me ?

0 Likes
1 Solution
Bob_Marlowe
Expert II

In main.c read the comments

/* Comment the following line to disable the tuner. This allows

* the project to operate in a stand-alone fashion without connecting

* the I2C tuning interface */

/* #define ENABLE_TUNER  */

Remove the comments and it will work.

Bob

View solution in original post

0 Likes
1 Reply
Bob_Marlowe
Expert II

In main.c read the comments

/* Comment the following line to disable the tuner. This allows

* the project to operate in a stand-alone fashion without connecting

* the I2C tuning interface */

/* #define ENABLE_TUNER  */

Remove the comments and it will work.

Bob

View solution in original post

0 Likes