cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

I'm trying to make a QR Code Scanner & Decoder.

   

I referred some material on Atmel's "SAM4S PIR Camera Reference Design" which uses a combination of PIR sensor + CMOS sensor to detect motion & take a VGA-compatible snapshot respectively.

   

The CY8CKIT-048 also has a PIR sensor. I want to know if a CMOS sensor can be used to obtain a similar functionality.

   

My primary objective is a QR code scanner, so, higher resolution is not a necessity.

   

Also, please let me know if there are other ways to do so using the CY8CKIT-048 or any other PSoC.

   

 

   

 

   

 

   

====================================================================================

   

Links to files:

   

"AT01180: Barcode and QR code scanner User Guide" - http://www.atmel.com/tools/SAM4S-WPIR-RD.aspx?tab=documents

0 Likes
1 Reply
EmHo_296241
Contributor II

Hi,

I think PSoC 4 device in CY8CKIT-048 kit doesn't support CMOS image sensor because of limited clock speed gpio speed. It does not have any UDB blocks. The device can support PIR sensor, but it may not your purpose.

0 Likes