cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

chmoc_1567941
New Contributor

how can i program standalone psoc-4 IC???

   

is that necessary to use HSSP method to program psoc-4??

0 Likes
8 Replies
Bob_Marlowe
Expert II

Three different choices:

   

A professional programmer

   

A Miniprog3. Needs a 5 pin or a 10 pin connection

   

A KitProg which is part of some prototyping kits as a snap-off part, needs a 5 pin interface too.

   

The latter two solutions allow for debugging in case that this is wanted.

   

 

   

Bob

0 Likes
chmoc_1567941
New Contributor

Thanks bob for fast responce,

   

what is the better solution for production level in this three???

0 Likes
chmoc_1567941
New Contributor

is there also need Psoc-5 as a debugger in this three??

   

i want to program directly to the psoc-4.

0 Likes
Bob_Marlowe
Expert II

is there also need Psoc-5 as a debugger in this three?? I don't know exactly what you mean with that.

   

what is the better solution for production level in this three??? That depends on how many "production level" are. High volumes could be programmed by Cypress directly or they could recommend an institution.

   

Professional programmers are expensive, but they (usually) are able to program anything (except your TV setup 😉

   

The MiniProg3 is good for ~100 volumes.

   

The Kitprog has got no housing and requires some soldering when made ready as a programmer. Very cheap, so you might use several of those in parallel.

   

 

   

Bob

0 Likes
chmoc_1567941
New Contributor

i attached one picture. i found from community.

   

can i apply same for program external psoc-4 ic???

0 Likes
Bob_Marlowe
Expert II

Tis is the kitprog of the pioneer board which cannot be snapped off. Modifications may damage your pioneer kit.

   

Better use a CY8CKIT-043 PSoC4 M prototyping kit. There is a brief documentation concerning the kitprog.

   

 

   

Bob

0 Likes
chmoc_1567941
New Contributor

i used this method to program psoc-4 around 20 times but after that i faced problem like this:

   

There was an error while programming the device: Connection with device lost during programming. Verify the device is connected and try again.

   

can we solve this or my board is permenantly fail??

0 Likes
Bob_Marlowe
Expert II

i used this method...   Which method?

   

Remove USB driver from port using USBdeview from nirsoft (free), reboot system, plug in kitprog and wait until drivers are downloaded and installed again

   

 

   

Bob

0 Likes