cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hello!

So I'm in my first year of messing around with a PSoC and have gotten the CY8KIT-042 pioneer kit.

As project I'm trying to get the PSoC the be programmed by the ESP.

I've gotten it to work so it would flash over USB but I honestly have no idea on how to start this project with the ESP.

Any help? Thanks in advance ^.^

0 Likes
1 Solution
3 Replies
EvPa_264126
Valued Contributor II

If CY8KIT-042 is connected - you will see KitProg USB-UART (COMxx) in Device Manager.

This means that you have a COM port on the J8 connector.

Tx:  PSoC 5LP P12  [7] (on J8)

Rx:  PSoC 5LP P12  [6] (on J8)

eg:

https://www.element14.com/community/message/75846/l/psoc-4-pioneer-kit-community-project04--usb-uart...

UART.png

Anonymous
Not applicable

Yes I got this to work so that I can flash the board via USB but now I wanna try to get it so it flashes trough the ESP8266 is this possible?

0 Likes