cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

ErBU_1372276
New Contributor II

Hi,

   

I have a time of 500ms between reset and calling the main function. It is the function in start_c init_libc_array taking all this time? How to reduce this time?
I created a test project for moving only one output to test this time.

   

Thank you,

   

Eric

0 Likes
1 Solution
Bob_Marlowe
Expert II

All the programming of the internal registers which include components and wiring is done after stabilization of the clocks and PLL. All registers get a value, so setup time is independent of the components used,

   

In cydwr-file, System tab there is a "Device Configuration Mode" setting which allows for using more flash but faster setup.

   

 

   

Bob

View solution in original post

0 Likes
3 Replies
Bob_Marlowe
Expert II

All the programming of the internal registers which include components and wiring is done after stabilization of the clocks and PLL. All registers get a value, so setup time is independent of the components used,

   

In cydwr-file, System tab there is a "Device Configuration Mode" setting which allows for using more flash but faster setup.

   

 

   

Bob

View solution in original post

0 Likes
ErBU_1372276
New Contributor II

thank you for your help, I'll try.

0 Likes
ErBU_1372276
New Contributor II

Thanks Bob,

   

I disable the WCO clock and now I have 5ms between reset and the main function.

   


Thank you again for your help.

   

Eric
 

0 Likes