cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

AMSH_1344256
New Contributor

DEAR READER

   

I am going through the PSoC 4 development kit User guide and need to know what is the significance of capacitor Ctank and Cmod in the module.

   

thanks and regards

0 Likes
3 Replies
ETRO_SSN583
Esteemed Contributor

Used in Capsense designs -

   

 

   

www.cypress.com/

   

 

   

The CY8CKIT-049 prototyping kits are also CapSense enabled as both the CMOD and CTANK capacitors necessary for CapSense and CapSense Proximity designs are loaded by default.

   

 

   

Regards, Dana.

0 Likes
AMSH_1344256
New Contributor

thanks

   

means if  i want to use Capsense feature i need to install Cmod and Ctank. otherwise they are not required.

   

AMIT

0 Likes
Bob_Marlowe
Expert II

The CTank and CMod are already installed, so when you want to use CapSense on your BLE Kit you do not have to modify anything. When using the pins for other purposes just keep in mind the extra capacity which will not be of any concern in most of the cases.

   

 

   

Bob

0 Likes