- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hello,
I am designing a 9 position slider as recommended in the AN85951 document. The figure 7.15 shows a typical linear design with two dummy segments at the ends of the slider (see the attached file). The segment are surrounded by the hatch with an air gap.
In case of the hatch is connected to GND, can I connect the two dummy segments to the hatch or do i have to route a specific trace?
thank you
Solved! Go to Solution.
- Labels:
-
PSoC 4 MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hey @GeFLo,
> Yes, you may connect the two dummy segments to the hatch.
> The dummy sensors are highly recommended. They maintain linearity among all the individual sensors present in the slider.
[refer to your Capture002.PNG attachment]: When a single sensor is being scanned, other sensors are connected to GND or shield (as the case may be). All the sensors from SLD1 to SLDn-2 will have one such sensor on either side. To maintain the same for the end sensors SLD0 and SLDn-1, dummy sensors are essential.
Regards,
Nikhil
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
Hey @GeFLo,
> Yes, you may connect the two dummy segments to the hatch.
> The dummy sensors are highly recommended. They maintain linearity among all the individual sensors present in the slider.
[refer to your Capture002.PNG attachment]: When a single sensor is being scanned, other sensors are connected to GND or shield (as the case may be). All the sensors from SLD1 to SLDn-2 will have one such sensor on either side. To maintain the same for the end sensors SLD0 and SLDn-1, dummy sensors are essential.
Regards,
Nikhil