cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

user_289226
New Contributor

Has anyone had any luck getting a Fordata MCOB21605GX 16x2 OLED (using 4-bit OLED1311 controller) display working, who could help? I have been using LCDs for bar graphs & text, but this OLED is simply not playing!

Thankyou

0 Likes
1 Reply
Rakshith
Moderator
Moderator

Hi user_289226​,

I do not have the OLED module that you are referring to. Can you tell me what the issue is? If the program is getting stuck, you can attach to the running target and check the call stack to see where the program is stuck. You can also debug the code.

Also, you can find the program to interface OLED 1306 in this thread - Re: How to interface an SSD 1306 OLED?

Hope it helps,

Regards,

Rakshith M B

Thanks and Regards,
Rakshith M B
0 Likes