Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

What MCU can be used to program PSoC4 chips (4200 L series) ? 

0 Likes
1 Solution
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I question if it is possible measuring distances using capsense. Capsense was made to detect human body pressing a switch or approaching a sensor wire. Quite more than a 2mm distance measure of a pad. Enter "capsense layout" into the keyword search field at top of this page and read...

   

btw: It is always advisable to use a prototype kit at first. There is a programmer / debugger interface attached and you will easily see results. When your prototype runs you may think about making your own pcb.

   

 

   

Bob

View solution in original post

0 Likes
7 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

The answer must be "Any MCU can program a PSoC" 😉

   

Probably you'd like to know what kind of Programmer you need. There are two choices:

   

Use a Miniprog3 which is the cleanest solution. no self-made hacks, it works out-of-the-box for every PSoC.

   

Use a Kitprog which is a snap-off part of all the prototype kits that allow for debugging as the CY8CKIT-043.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hello bob,

I am trying to build a proximity sensor using the PSoC4 MCU IC. I would like to build it using the IC instead of the prototyping kit (preferably) given my design conditions - refer to the attached image.

   

http://i.imgur.com/qB4a2bl.jpg

   

 

   


I need to measure the distance between the surfaces A and B through proximity sensing. I will build the proximity sensor on one of the surfaces and connect it to the PSoC device.

My concern is how do I interface it with other periferals such as the computer ? what other parts do i require with the IC to complete the board? how do I program the PSoC to get the real time proximity distance/changes in it?

   

 

   

P.S. :- I am a novice in embedded and hardware design. If I am wrong in certain case please let me know.

 

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

I question if it is possible measuring distances using capsense. Capsense was made to detect human body pressing a switch or approaching a sensor wire. Quite more than a 2mm distance measure of a pad. Enter "capsense layout" into the keyword search field at top of this page and read...

   

btw: It is always advisable to use a prototype kit at first. There is a programmer / debugger interface attached and you will easily see results. When your prototype runs you may think about making your own pcb.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Thanks Bob.That was helpful. But, is capsense only designed to detect human skin? Can it work against plastic as well?

   

My constraints were such that I had to design a pcb and connect to the sensor pad on the plastic surface. But I will try the prototyping kit first then. 
But in that scenario can I have copper pad/trace on the surface and connect it to the i/o of the kit? Will that work ? or is the sensor pad only on kit itself?

   

Thanks 
Aman

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

On a prototyping kit as the CY8CKIT-043 PSoC M Prototyping Kit are no copper traces for capsense. So you are free to design your own buttons. I used some conductive ink on overhead foil. Worked!

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hey bob, thanks again. I will connect the pin to a copper tape over the plastic gripper.

   

Another question - I believe that I can get analog values through the kit, but what will be the resolution of measurement? or what is the minimum 'displacement change' i can measure and what are the min. and maximum distances I can obtain from this system?

   

 

   

Regards,
Aman

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Best is to install the kit software (Creator 4.1) first and go through the components for your selected chip. Every component has got a datasheet which describes its function, APIs and -when appropriate- AC and DC characteristics.

   

 

   

Bob

0 Likes