cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hello

Is there a flash programmer for the CY8KIT-049-42XX board which runs under Linux/OSX?

Or is the PSoC Creator the only way to do it?

0 Likes
1 Solution
3 Replies
Bob_Marlowe
Expert II

You do not need a flash programmer. Programming is done by the bootloader program that is already set up in your chip.

What you need is a linux Bootloader host. I don't know if there is one. Enter "linux bootloader host" into the keyword search field, there are some matches.

Bob

0 Likes
Anonymous
Not applicable

Seems like this might be a good start:

C:\Program Files (x86)\Cypress\PSoC Creator\3.3\PSoC Creator\cybootloaderutils

From the readme.txt:

This directory contains the source files for the Cypress-provided Bootloader Host Tool, which is used test out the bootloader running on a PSoC chip. For more information about this tool, refer to the Bootloader Host Tool documentation (F1 from the application). For more information about the source code in this directory, refer to the Bootloader Component Datasheet."

0 Likes