cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

frro_3974886
New Contributor II

On CY8CMBR3116-LQXIT is the pull-up on HI/BUZ/GPO7 mandatory ?

When HI/BUZ/GPO7 is used as inetrrupt (Active LOW) is a Floating output when HIGH ?

Or the pull-up is to avoid false triggering when powering up the device ?

0 Likes
1 Solution
Hari
Moderator
Moderator

Hi frro_3974886

Yes, a pull up is mandatory on the HI line. The default configuration of the pin is open drain drives low. Hence, it is pulled LOW to indicate an interrupt to the user, but is left floating otherwise.

Hence, a pull up is mandatory.


Thanks,

Hari

View solution in original post

0 Likes
1 Reply
Hari
Moderator
Moderator

Hi frro_3974886

Yes, a pull up is mandatory on the HI line. The default configuration of the pin is open drain drives low. Hence, it is pulled LOW to indicate an interrupt to the user, but is left floating otherwise.

Hence, a pull up is mandatory.


Thanks,

Hari

View solution in original post

0 Likes