Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi im new to this community and just got a cy8ckit-42 and have lots to learn.

   

 My main reason/project is to make a controller for my Fishtank Led bars.

   

So im not sure where to Start but I need to make a Ir decoder then a Sender to control them.Does anyone have a Example or can help with this Project?

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

Welcome in the forum, Eric!

   

So you will have to get another PSoC kit for the receiver. I would suggest you to purchase a CY8CKIT-043, cheapest solution.

   

You'll need a photo diode connected to the PSoC and probably an amplifier for the (weak) signal. Have a look at the -043 schematics how to do that, for the programming there is an example project (in Creator Start Page -> Kits).

   

For the Sender I's suggest to use a PWM component triggering an IR LED with a frequency of  ~1-2kHz to make it easy to distinguish the signal from ambient light.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Could i use a board like this one to just receive/send a signal instead? Its 5v and uses ttl

   

http://www.ebay.ca/ulk/itm/281827852550 

0 Likes
HeLi_263931
Level 8
Level 8
100 solutions authored 50 solutions authored 25 solutions authored

A while back there was also a discussion about how to implement a RC5 decoder. Look in the forums for it, it might be helpful.

0 Likes