cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC™ 4

1 Solution
MotooTanaka
Esteemed Contributor

Hi

Since I had a sample FreeRTS Project for CY8CKIT-044 (Flash 128KB, SRAM 16KB)

I changed the device to CY8C4247LQI-BL483 (CY8CKIT-042-BLE) and added a BLE module

in the schematic. I only called CyBle_Init() and did nothing more with BLE.

012-ble_schematic.JPG

First the good news is, yes, I could compile the project and FreeRTOS seems to be working!

010-FreeRTOS-test.JPG

Second the bad news is, the device is almost FULL!

011-Build-Done.JPG

It says the SRAM used is 99.1% !

So I wonder if we can do any useful thing on top of this.

I would recommend you to get and use CY8CKIT-042-BLE-A,

which has CY8C4248LQI-BL583 (Flash 256KB SRAM 32KB),

So that some more things can be done 😉

moto

View solution in original post

0 Likes
2 Replies