cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

StWa_1982846
New Contributor II

The PSoC4 4200 BLE part found in the CY8CKit-042-BLE-A has an Environmental Sensing profile (ESS) available in the BLE component. I'm still trying to find my way through the mass of structures and definitions. Comparing the ESS to the HTS (Health Thermometer) just confuses one all the more. Does anyone have example code for use of the ESS? I am trying to build up a system of multiple sensors reporting to a client using the 4200.

Steve

0 Likes
1 Solution
rola_264706
Honored Contributor II

Here is an example program and it has a PDF file with information on the program. I am running PSoc Creator   4.2 (4.2.0.641).

View solution in original post

0 Likes
2 Replies
rola_264706
Honored Contributor II

Here is an example program and it has a PDF file with information on the program. I am running PSoc Creator   4.2 (4.2.0.641).

View solution in original post

0 Likes
rola_264706
Honored Contributor II

Here is a program that reads Battery voltage and Die Temperature but you could use it to read another sensors.

0 Likes