cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

JoWi_3984961
New Contributor II

I see readelf.exe is in the PSoC Creator directory structure after installing it.  How to use it to generate a symbol table (for use by custom tool we need) that can be human readable or at least simple to machine read?  Need the RAM globals', the ones that do not move around, addresses handy for other tools.  I tried to run readelf.exe, but Windows 10 did not recognize it as a program it could run.

Do I need to use a bash shell?

PSoC 4 application..

0 Likes
1 Solution
DheerajK_81
Moderator
Moderator

Its not clear when you want to run it. If you want to run the readelf.exe after the build step in PSoC Creator you can go to Build Settings > ARM GCC Compiler > User Commands > Post Build and type the following:

pastedImage_3.png

"C:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\import\gnu\arm\5.4.1\arm-none-eabi\bin\readelf.exe" -s "${OutputDir}\Design01.elf

Here ${OutputDir} is a macro you can use to point to the Output directory where the elf is located. "Design01.elf" is the name of the elf file in my case. It will be based on the project name.

pastedImage_0.png

You can use bat files to execute the above command. Just provide the complete path to readelf and to the elf file.

Regards,

Dheeraj

View solution in original post

0 Likes
3 Replies
DheerajK_81
Moderator
Moderator

Its not clear when you want to run it. If you want to run the readelf.exe after the build step in PSoC Creator you can go to Build Settings > ARM GCC Compiler > User Commands > Post Build and type the following:

pastedImage_3.png

"C:\Program Files (x86)\Cypress\PSoC Creator\4.2\PSoC Creator\import\gnu\arm\5.4.1\arm-none-eabi\bin\readelf.exe" -s "${OutputDir}\Design01.elf

Here ${OutputDir} is a macro you can use to point to the Output directory where the elf is located. "Design01.elf" is the name of the elf file in my case. It will be based on the project name.

pastedImage_0.png

You can use bat files to execute the above command. Just provide the complete path to readelf and to the elf file.

Regards,

Dheeraj

View solution in original post

0 Likes
JoWi_3984961
New Contributor II

I would like to run it from a command line. Which shell is required?

0 Likes
DheerajK_81
Moderator
Moderator

You can run the commands using Command Prompt.

Regards,

Dheeraj

0 Likes