cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hello,
I'm wondering if it is possible to modify the timeout interval between sending a Write Request (using CyBle_GattcWriteCharacteristicValue) and getting CYBLE_EVT_TIMEOUT event in case the Write Response is not received. The default timeout seems to be 30 seconds, which is a bit too long for our application. Changing cyBle_connectingTimeout has no effect (it works for connection timeout, though).

   

We are using CYBLE-022001-00 and BLE component v2.30 in PSoC Creator 3.3 CP2.

   

Thank you in advance!
BR - Stefano Voulaz

0 Likes
1 Reply
Anonymous
Not applicable

Hi,

   

This is fixed by the Spec as 30 seconds. This cannot be changed.,

   

Regards,

   

- Madhu Sudhan

0 Likes