I want to display finger position on the LinerSlider with a value between 0 and 100.
I'm using UART and TeraTerm to display the value.
Here's the main reference video (URL: https://www.youtube.com/watch?v=fsxwYpacrCA&list=PLIOkqhZiy83F8KPvHejA4ujvAfwJYpAtP&index=13).
I think it's because this video is old, but some functions are not provide such as
CapSense_ScanEnableWidgets()
, and the ID of the LinerSlider is different.
I have specified ID "CapSense_LINEARSLIDER0_WDGT_ID" instead of ID "CapSense_LINEARSLIDER0__LS".
(CapSense_P4_v7_0.pdf Page67 said to do so here, so I did).
UART connection is OK, but It doesn't display the value of finger position.
Please look at my project I shared and tell me what is wrong with it.
Solved! Go to Solution.
Hi @wangyuanfan,
CapSense_Start() function call is necessary to initialise the CapSense modules. This function call also scans the widgets, initialises the firmware filters and updates the baseline. Always use CapSense_Start() function call at the start of the application.
After scanning the widgets, the data needs to be processed. Use CapSense_ProcessAllWidgets() function for the same. The baselines get updated too.
Find the project archive attached.
Regards,
Nikhil
Hi @wangyuanfan,
CapSense_Start() function call is necessary to initialise the CapSense modules. This function call also scans the widgets, initialises the firmware filters and updates the baseline. Always use CapSense_Start() function call at the start of the application.
After scanning the widgets, the data needs to be processed. Use CapSense_ProcessAllWidgets() function for the same. The baselines get updated too.
Find the project archive attached.
Regards,
Nikhil
It worked correctly! Thank you so much!!