cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

RuDe_666331
New Contributor II

I used the BLE_HID_mouse example and adapted some lines to get the mousewheel data as 4th byte:

   

#define MOUSE_DATA_LEN              (4u)  //instead of 3

   

and added:

   

abMouseData[3u] = bScrollWheel_value; (I tested 120 or -120)

   

 

   

Also in the BLE component HID-profile I changed:

   

  - "Human interface device"

   

        - "Boot mouse input report: Boot mouse input report value"  from 3 to 4 bytes  to include the extra wheelvalue byte

   

        - "Report In: Report value" also from 3 to 4 bytes  to include the wheel byte

   

 

   

No errors, and I even see in cysmart on my PC that the 4th byte is being transmitted and it's received correctly.

   

But it doesn't seem to scroll, what am I doing wrong, maybe a Bug in version 3.1 SP3 or some characteristics needs to be reported?

0 Likes
1 Reply
RuDe_666331
New Contributor II

 Found the solution myself:

   

- In the BLE-component in reportmap added the "wheel" parameter after the X & Y and below put "report count" on 3 instead of 2

   

Also important on Android: always go to All aplications and under the Bluetooth App. clean Cache and delete data.

0 Likes