Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Anonymous
Not applicable

Hi,

   

I have some dubts about the Proc.

   

what I do with the pins not used the EZ-PROC? How do I set to prevent the leakage current.

   

Leds can connect directly to the pins of the EZ-PROC? He can provide necessary current to light LEDs? If so, which pins can I use?

   

 

   

Thank you!

0 Likes
3 Replies
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

You may connect an LED to any GPIO pin using a limiting resistor. A pin is able to drive 4mA and to sink 8mA, look into the pin's datasheet where all ratings are listed. Do not exceed the total power dissipation of the chip.

   

Unused (and unprogrammed) pins are in a high-Z state which may pick up some noise, so you may connect them to GND.

   

 

   

Bob

0 Likes
Anonymous
Not applicable

Hi Bob, thanks for your reply. I need the pins not used to use a resistor to GND or can link them directly on GND?

0 Likes
Bob_Marlowe
Level 10
Level 10
First like given 50 questions asked 10 questions asked

High-Z impedance does not need a resistor when connected to GND.

   

 

   

Bob

0 Likes