cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hello Guys,

   

1) I am not able to find any example code that creates network of at least 8 CYBLE-222014 devices. I found following example designed for different BLE chips and not able to make itt working with CYBLE-222014.

   

https://github.com/cypresssemiconductorco/PSoC-4-BLE/tree/master/100_Projects_in_100_Days/Project052...

   

https://github.com/cypresssemiconductorco/PSoC-4-BLE/tree/master/100_Projects_in_100_Days/Day049_BLE...

   

2) My other question is whether or not it is possible to create star network ( 1 Central and 8 peripheral ) connectivity of 8 BLE devices.

0 Likes
1 Reply
Anonymous
Not applicable

Hi,

   

Those projects use the Prism, Glitch filer components  which are not supported by the CYBLE-0222014-00 module. Also, p2.5 and p2.7 pins used in the project are not present in CYBLE-0222014-00  module. So the project did not work.

   

So, you need to remove this components and modify the firmware accordingly. Other than this, the same algorithm can be used for CYBLE-0222014-00 for creating a mesh. you can create a Star network as well. However, our device support only one connection at a time , so the connection and disconnection must happen in a time multiplexed way.

   

Regards,

   

-Madhu Sudhan

0 Likes