Announcements
Community Announcement : Welcome to the NEW Cypress Developer Community.
cancel
Showing results for 
Search instead for 
Did you mean: 

PSoC 4

Anonymous
Not applicable

Hello,

   

I have to build a project with IAR (version 7.80.4 using a commercial license). The project is set-up with PSoC Creator 4.1 and then connected to IAR via the Project->Export to IDE. Since adding the CapSense [v4.0] component I get the following error:

   

Error[Li016]: size limit exceeded. The application needs 0x1a29a (107 162) bytes, which is greater than the limit of 0x8000 (32 768) bytes.
            The limit is due to license "ARM.EW.LINKER" from "CapSense_SmartSense_SL_v3_10.o(Capsense_P4Library_IAR.a)" (and 1 other module).

   


It seems like a component (Capsense_P4Library_IAR.a) was put together with the Kickstart edition of IAR? 

   

After taking out the CapSense component everything is fine in IAR and the application still needs more than 100kbytes.

   

What can I do to make it work (I have to use IAR instead of PSoC creator)? 

   

Thanks

   

Thomas

0 Likes
3 Replies
Anonymous
Not applicable

So, given that the project you are using is taking up 100 kB, and your device only supports 32 kB, you think there is a solution without cutting out hundreds of lines of code? Not likely. If your device really only supports 32 kB of space, then you will need to keep cutting out code/components, or increasing optimization (-o3 is usually the max compression iirc). Otherwise, you need a bigger chip 🙂

0 Likes
Anonymous
Not applicable

Hey,

   

the limit does not come from the device. As I said in the first post, without the CapSense Component the project still consumes more than 100 kB and I can build and flash and debug with IAR without any problems.

   

It seems like the code size limit is imposed by the Cypress library for the CapSense v3.1 block "CapSense_SmartSense_SL_v3_10.o(Capsense_P4Library_IAR.a)".

   

Anyway the CapSense v3.10 block was from PSoC Creator 4.0 update 1. After updating the PSoC Creator to Version 4.1 I used the CapSense v4.0 block. Somehow the reference to the older CapSense library was not removed automatically from the IAR project but after taking out this reference, everything is fine now.

   

Thanks

   

Thomas

0 Likes
Anonymous
Not applicable

Ah, sorry for the misunderstanding. I thought you were trying to shove a 100 kB project into a 32 kB device >.<

   

I think when installing new PSoC creator versions it leaves the older versions to allow for multi-version development. Thus, I would suspect that you didn't uninstall the PSoC 4.0 once you got the PSoC 4.1 installed. Glad you figured out the problem though!

0 Likes